Organize the imported tags
Organize imported tags into folders. The imported tags remain synchronized with the controller after moving them into different folders.
Important: Rockwell Automation does not recommend separating and reorganizing the tags contained in a structured tag because the initial tag structure is restored if the tag is resynchronized.
Prerequisites
To organize the imported tags
- In Project view, navigate to Tags under a Communication station.
- To create a folder, right-click the Tags object and select .
- Drag the imported tags into the folder.