Communication drivers overview
Some communication drivers may have specific characteristics.
| Communication driver | Online tags import | Offline tags import |
|---|---|---|
| Modbus driver | ||
| MELSEC FX3U Driver | ||
| S7TCP driver | ||
| OMRON EtherNet/IP driver | ||
| MELSEC Q driver | ||
| S7 TIA PROFINET driver | ||
| OMRON Fins Driver | ||
| CODESYS Driver | ||
| TwinCAT driver | ||
| Serial port | ||
| RA EtherNet/IP Driver | ||
| Micro Controller Driver |
* Only for selected controller series. For more information, see S7TCP driver.