Set dynamic variables polling time for controllers
Set the time interval between readings of tag values from controllers at runtime.
-
In Project view, select NativePresentationEngine or WebPresentationEngine.
For more information, see Presentation engines.
-
In Properties, set Dynamic variables polling time.
Tip: Set the polling time between one sampling and the next in HHHH:MM:SS.MS format.