Micro Controller Driver

Observe these guidelines when working with Micro Controller Driver.

Supported controllers

Micro Controller Driver supports Micro800™ controllers and MicroLogix™1400 controllers.

Controller tags import

With Micro Controller Driver, you can import tags from Micro800 controllers in the online mode.

Data types

Micro Controller Driver supports these data types:

Table 1. Basic data types
Datatype FactoryTalk Optix datatype

BOOL

Boolean

SINT

SByte

DINT

Int32

REAL

Float

STRING

String

LREAL

Double

INT

Int16

LINT

Int64

USINT

Byte

BYTE

UINT

UInt16

WORD

UDINT

UInt32

DATE

TIME

DWORD

ULINT

UInt64

LWORD