Open a remote project
Open a remote project to view a shared project that other users edit.
Pull the changes that other users make to see the latest version of the project before incorporating the changes or making any additional changes.
-
If there is an open project, select
Project and then select Close Project.
- Select Close or if there are changes to save, select Save and close.
- On Create a new project, select Open and then select Remote.
-
On the Start page, complete:
- Select Open. "Opening project from remote" appears in the status bar and the new project opens with the same name as the remote repository.
-
If, in the main toolbar,
Pull from remote is blue and contains a number, the project has committed changes on the remote repository that you need to pull in order to see the latest version of the project. The message "Remote changes available to pull" appears in the status bar.
-
Select
Pull from remote. The message Pulling project from remote appears in the status bar.
Any conflicts between changes in the remote repository and changes in the local project appear highlighted in Pull preview. Green rows in Pull preview show changes from the remote repository, not conflicts. - In Pull preview, expand a highlighted conflict to display values that are in conflict.
-
Select the version of content to keep:
-
Individual local change. In a highlighted row, select
Local history on the left. - All local changes. At the top of the preview, select Take all local.
-
Individual remote change. In a highlighted row, select
Remote history on the right. -
All remote changes. At the top of the preview, select Take all remote.
Tip: An icon in a row in Pull preview indicates:A conflict exists between the local and remote project.
A conflict was resolved by selecting either the local or remote change in the row.
A change exists in the local or remote project.
An object was added.
An object was removed.
-
- Select Accept and push to accept the selected changes, or select Cancel to reject all of the conflicts in the remote project and retain the values in the local project.