Users
Users appear as objects in Project view. Assign permissions and roles to users to determine the content and interface that the user sees in the application at runtime.
Each project has a default Anonymous user that authenticates the application session. At runtime, the session user is the user who is logged on to the application. The content and UI that appears depends on the visibility set for a group of users or users with a specific role. See Configure security for content at runtime.
Tip: To allow local and domain users to log on, see Authentication.