Change user properties
Change the properties of a user to modify the domain, password, location, and language for that user.
- In Project view, expand Security.
- Expand Users.
- Select a user.
-
In Properties, change:
- Name. Name of the user.
- Password. Password that the user must provide to log on to the application.
- Locale. Location of the user.
- Languages. Language configured for the user.
- Measurement system. The measurement system used to display data to the user:
- International system of units
- US customary measurement system
- British imperial units
- Domain. Identifies the local Windows® user account for a domain-linked user account.