Configure non-standard units of measure
You can configure non-standard units of measure in the Engineering Units Dictionary. Using non-standard units of measure you can, for example, express the number of pieces produced in one hour in beats per minute.
Non-standard units of measure have specific properties. Slope is the conversion coefficient to convert the standard unit value to the non-standard unit. Intercept is the value to add to the referenced unit of measure. The conversion is performed using the linear expression Y = M x X + Q where X is the input value, M is the slope, and Q is the intercept that calculates the Y output result
- In Project view, right-click Model.
- Select .
- Select Engineering unit dictionary.
- Double-click the new dictionary.
-
In the title bar of MeasurementSystemMap that opens in the center of the screen, select
.
A new row appears in the map table.
-
In the Physical dimension column, select the reference quantity for the non-standard unit of measure.
For example, for the beats per minute, select .
- In the Display name column, type the name of the unit of measure.
-
In the Description column, type a description for the unit of measure.
Tip: Name and Description are both translatable through the LocalizationDictionary object.
-
In the Slope column, enter the conversion coefficient for the standard unit value.
For example, enter 60 to calculate beats per minute.
-
In the Intercept column, enter the value to add to the referenced unit of measure.
For example, enter 0.
- Physical quantity. Frequency.
- Display name. BPM.
- Slope. 60.
- Intercept. 0.