Configure a recipes editor
You add a recipes editor widget by selecting it from the template libraries and editing its properties.
Tip: You can develop your own recipes management solution. For more information, see Recipes editor customization.
Prerequisites
To configure a recipes editor
-
From the toolbar, select
Template Libraries.
-
In Template Libraries:
- Select Widgets.
- Drag Recipes Editor to the UI folder in Project view.
- Select Close.
-
In Project view, double-click RecipesEditor.
The widget preview displays in the central pane.
- In Properties, in the RecipeSchema property, select a Recipe Schema object.
- In Project view, automatically configure the graphical objects and dynamic links used to assign values to ingredients at runtime by right-clicking the RecipesEditor object and selecting Execute Setup.
The ingredients list appears in the widget.
Do any of the following: