Configure a recipe schema
-
From the toolbar, select
Open dashboard page.
- In the central pane, select Configure a recipe.
-
Select an existing recipe or create a new recipe:
-
To create a recipe:
-
Select New recipe.
-
Edit Name.
-
Complete Target node.
The target node defines the recipe schema ingredients. The target node can be any project node that contains the desired variables.
For example, the target node can be:-
The Model folder
-
An object inside the Model folder
-
A node that contains variables from one or more controllers
Tip: In a complex project, to define variables contained in several nodes as ingredients of a recipe schema, create a dedicated object in the Model folder and add variables inside it. Then, create a dynamic link between the variables and the ingredients. If the object is selected as the target node, the selection of the recipe schema ingredients is intuitive because only the variables referenced in the object are displayed. -
-
Select Next.
-
-
To edit an existing recipe:
-
Select an existing recipe.
-
Edit the recipe properties.
-
-
To duplicate an existing recipe:Tip: Duplicating an existing recipe enables you to create a new recipe based on the existing recipe quickly.
-
Right-click an available recipe and select Duplicate.
- If needed, edit the recipe properties.
-
-
- Select Next.
-
Select an existing database or configure a new database:
-
To use an existing database:
-
Select an existing database.
-
If necessary, edit the database properties.
-
Select Next.
-
-
To create a database:
-
Select New database.
-
If needed, edit the Name and Type fields.
-
Select Next.
-
If necessary, edit the database properties.
-
Select Next.
-
-
To duplicate an available database:Tip: Duplicating an existing database allows you to create a database base on the existing database quickly.
-
Right-click an available database and select Duplicate.
-
If necessary, edit the database properties.
-
-
- Select Next.
-
Select the recipe parameters to use.
Tip: You can show or hide variables (parameters) nested in other variables by using the Nested variables toggle. You can quickly find the parameters that you want to select by using the Search field.
- Select Next.
- Review the settings.
- Select Exit.