Save a project
Save your project to save your progress. You can store projects locally, in a version control repository, on a network drive, or a removable drive.
Save the project using one of three ways:
-
From the toolbar, select
Save.
The project is saved to the same location from which you opened the project.
-
From the toolbar, select the down arrow after
, select Save As, and then in Save project as, complete:
-
From the toolbar, select .
The project is saved and a commit is made to the local version control repository.