Close a project
Close a project from the Start page.
You can have more than one project open at a time. When you open additional projects, additional instances of FactoryTalk Optix Studio open.
From the main toolbar, select
Project. On the Start page, select Close Project.
Tip: If you open the Start page from an open project and want to close the Start page, select
.