Edit an enumeration
Edit members of an existing enumeration object.
-
In Project view, double-click Enumeration#.
Enumeration editor displays in the central pane.
-
In the editor, manage the enumeration members:
-
To add a member, select
and complete:
- Value. Enumeration member value. Value is generally a consecutive integer.
- Display name. Name of the enumeration member.
- Description. Additional information about the enumeration member.
-
To edit a Value, Display name, or Description, double-click the corresponding cell and enter a new value.
-
To remove a member, select a cell in the corresponding row and select
Delete.
-