Create a template
Use a template to create objects, object types, and variables that have similar attributes.
-
Select
Template Libraries.
-
From Project view, drag the node into a library in Template Libraries.
For example, drag an object, object type, variable, or widget.
-
If prompted, resolve object type conflicts.
Type conflicts occur when object types of the new template duplicate object types of an existing template.
To address object type conflicts select either:- Skip. Do not update a specific object type. Keep the existing object type in the project.
- Replace. Replace a specific existing object type with a new object type.
- Rename. Rename a specific new object type with a unique name. Retain the existing object type.
- Skip all. Do not update any object types. Keep the existing object types in the project.
- Replace all. Replace all existing object types with new object types.
- Rename all. Rename all object types to with unique names. Retain the existing object types.
-
(optional) Select the template and enter a description.
For example, explain how to use or implement the object, object type, variable, or widget.