Import a template
Place a template in a node in Project view to add the object, object type, or a variable to the project.
Tip: If the template is a graphic object, you can drag the graphic element from the library to the editor.
-
From the main toolbar, select
Template Libraries and either:
- Drag a template from the library into a node in Project view.
- Drag a graphic object template from Libraries to the editor or Project view.
-
If the template is an object type, select either:
- Import as type. Add an object type based on the template into the project.
- Import as instance. Add an object instance based on the template into the project.