Import fonts
You can configure your FactoryTalk Optix Application to use custom fonts in TTF or OTF format. To use a font other than a default, import the font into the project to make it available as an object property.
Tip: If you use FactoryTalk Optix Studio desktop editor, instead of performing this procedure, you can copy custom TTF or OTF font files into the ProjectName\ProjectFiles\Font folder.
-
In the main toolbar, select
Browse project files.
-
In Project Files, select
Import file(s).
-
Navigate to and select the font to import and then select Open.
Verify that the font selected for the project is available on the device and supports the required characters.
- Close Project Files.