Apply a global style to the project
Select a style sheet for a FactoryTalk Optix Application to display at runtime.
Prerequisites
-
Configure a global style in a stylesheet. See Configure a style sheet.
To apply a global style to the project
- In Project view, select either NativePresentationEngine or WebPresentationEngine.
- In Properties, in Style sheet, select the drop-down arrow after the style sheet value and then select the style sheet to apply.
The project uses the Global Style properties from the selected style sheet.