Configure a style sheet
Set Global Style to edit the styles applied to all graphic objects. Set Control Styles to edit the styles applied to specific control objects. Control styles overwrite the global style.
-
In Project view, select the style sheet to edit.
Tip: You can select the default style sheet, add a predefined style sheet, or create your own style sheet. See Add a predefined style sheet or Create a style sheet.
-
To set the global style that applies to all graphic objects, in Properties, under Global Style, select
and enter the values.
Tip: You can create dynamic links instead of entering the values manually. See Create dynamic links. -
To create a control style, under Control Styles, next to Object styles, select
.
For example, create a control style for switch objects.
-
To rename a control style, hover-over the style name, select
and enter a new name.
-
To edit a control style, expand Object styles, expand the style name, and then edit the properties by selecting
and entering values.
Tip: You can also create dynamic links instead of entering the values manually. See Create dynamic links. -
To delete a control style, next to the style name, select
Delete.