Edit an image
Edit an image on the canvas to edit the picture that appears in the image object.
- From Project view, double-click MainWindow (type) to open the editor in a separate tab.
- On the canvas, double-click the image you want to change.
Note: You can also edit an image from Project view by double-clicking the image in Project view to open a tab in the editor.
- In Select file, select the image to display and then choose Select.
Tip: If the image does not appear in Select file, select
Import file(s)and in Import file(s), select the image to import and then choose Select.