Add an image
Add an image to the canvas to insert an empty image and then specify the image the object is to display. You can change the image that the object displays.
- In Project view, right-click the object or folder to contain the image and then select .
- Double-click the empty image
that appears on the canvas.
Tip: If you resize the image to make it larger, the messageDouble click to select a picture
appears. - In Select file, select the image to display and then choose Select.
Tip:
To find items, start typing the item name to find in Select file.
If the file does not appear in Select file, select
Import file(s) and in Import file(s), select the file to import and then choose Select.