Multistate image
An object that can have multiple image states based on the input value. Each image state may reference a different image and may have a specific opacity. If the input value does not correspond with any image state, the default value is used (first defined state).
Example