Configure a dropdown button
Configure a Dropdown button object by linking it with a container object type.
-
In Project view, create a container object type to display when you select the dropdown button.
For more information, see Create a graphic object type.
For example, create a panel type.
- In Project view, in UI, right-click a container and select .
-
In Properties, create a dynamic link between the Panel property and the container object type.
For more information about dynamic links, see Create dynamic links.