String formatter
Modify the formatting of one or more values according to a customizable rule.
- Add characters before or after a value, if the value of the source variable is numeric.
- Format and parameterize SQL queries to use in database objects.
- Link multiple strings in a series.
- Apply numeric formatting, such as decimal places or float rounding.
Properties
| Property | Description |
|---|---|
|
Format |
The formatting rule for variable reference:
|
|
Mode |
The direction of the dynamic link:
|
Source
{index_number}placeholder- Progressive integer equal to or greater than zero. For example,
{1}
{#placeholder_identifier}placeholder- String prefixed with
#. For example,{#speed}
{index,alignment:format} to dynamically
change the formatting of the displayed data. For example:{0:f{1}}-
- The variable value linked with
{1}defines the number of decimal places.
- The variable value linked with
{0:{1}{2}}-
- The variable value linked with
{1}defines the numeric data type. - The variable value linked with
{2}defines the number of decimal places.
- The variable value linked with
{0,{1}:{2}{3}}-
- The variable value linked with
{1}defines the alignment. - The variable value linked with
{2}defines the numeric data type. - The variable value linked with
{3}defines the number of decimal places.
- The variable value linked with
Data types
| Format | Description | Example |
|---|---|---|
|
g |
Short date and time, local |
|
|
F |
Extended date and time, local |
|
|
X |
Short date and time, UTC |
|
|
x |
Extended date and time, UTC |
|
|
U |
Complete Universal Date and Time, UTC |
|
|
p |
Short date, local |
|
|
P |
Extended date, local |
|
|
d |
Short date, UTC |
|
|
D |
Extended date, UTC |
|
|
t |
Short time, local |
|
|
T |
Extended time, local |
|
|
h |
Short time, UTC |
|
|
H |
Extended time, UTC |
|
| Format | Description | Example |
|---|---|---|
|
d |
Numerical, without thousands separator. After the format placeholder, the number of decimal places is configured with an integer (without padding). |
|
|
n |
Numerical, with thousands separator. After the format placeholder, the number of decimal places is configured with an integer (without padding). |
|
|
e |
Exponential notation. After the format placeholder, the number of significant numbers is configured with an integer. |
|
|
f |
Fixed-point notation. After the format placeholder, the exact number of decimal places is configured with an integer. |
|
|
p |
Percentage. After the format placeholder, an integer is used to configure the number of decimal places. |
|
|
x |
Hexadecimal notation. |
255 ► ff |
|
b |
Binary notation. |
107 ► 1101011 |
|
o |
Octal notation. |
56 ► 70 |
| Format | Description | Example |
|---|---|---|
|
c |
Constant format. |
|
|
g |
General short format. |
|
|
G |
Extended general format. |
|
| Format | Description | Example |
|---|---|---|
|
l |
All lowercase. |
grüßEN ► grüßen |
|
u |
All uppercase. |
grüßEN ► GRÜSSEN |
|
t |
All first letters uppercase. |
grüßEN ► GRÜSSEN |
|
f |
Case independent. |
grüßEN ► grüssen |
| Format | Description | Example |
|---|---|---|
|
sql_identifier |
Formats a given String or LocalizedText as a table or column identifier. |
- |
|
sql_literal |
Formats the value of a variable as an SQL literal value (Number, String, date, time, and so on). |
- |
SQL queries examples
SELECT * FROM Table1 WHERE {0:sql_identifier} > 5
SELECT * FROM AlarmsDatalogger WHERE Time > {0:sql_literal}
LIKE operator:
SELECT * FROM AlarmsDatalogger WHERE Name LIKE '{0}'
SELECT * FROM Table1 {0}
0 is linked to a project string variable and parameterizes a column; The placeholder with index 1 is linked to a numeric variable that represents the value for the comparison operator >:
SELECT * FROM {0:sql_identifier} WHERE Column1 > {1:sql_literal}
LIKE operator:
SELECT {0:sql_identifier} FROM {1:sql_identifier} WHERE {0:sql_identifier} LIKE '{2}'
Path formatting
-
To format a string as a file path, you can use this syntax:
{index,alignment:filepath}.- Input
- ns=5;%PROJECTDIR%/Logo.svg
- Output
- C:\Users\UserName\AppData\Local\Rockwell Automation\FactoryTalk Optix\Emulator\Projects\ProjectName\ProjectFiles\Logo.svg
-
To format a string as a URI, you can use this syntax:
{index,alignment:uri}.- Input
- ns=5;%PROJECTDIR%/Logo.svg
- Output
- file:///C:/Users/UserName/AppData/Local/Rockwell Automation/FactoryTalk Optix/Emulator/Projects/ProjectName/ProjectFiles/Logo.svg
-
To format a part of a path, you can use this syntax:
file:///C:/Reports/Report{0}.pdf.
Inverse formatting
The inverse formatting feature allows you to modify a formatted value at runtime to replace the value with a new value that the application displays with the same formatting at runtime.
-
The dynamic link Mode of the converter must be Read/Write.
-
The Format field must have only one placeholder or source. The placeholder can have a suffix and/or prefix and be set with a format string such as
{0:n}.
Output
The string entered in the Format property, based on the formatting rules with values in place of the placeholder or placeholders.
Example

Read from the source node to the parent.
Write from the parent to the source node.
Read from the source node to the parent and write from the parent to the source node.