Engineering unit converter
Use the engineering unit converter to convert raw data values into scaled values based on a range of customizable values.
Properties
| Property | Description |
|---|---|
|
Raw min |
Minimum raw data value. |
|
Raw max |
Maximum raw data value. |
|
Scaled min |
Minimum converted value. |
|
Scaled max |
Maximum converted value. |
|
Mode |
The direction of the dynamic link:
|
| If... | Then... |
|---|---|
|
Raw min and Raw max properties are not set. |
The converter assumes that there is an analog variable set in the input via a dynamic link. Raw min and Raw max are set to Low limit and High limit of the input analog variable respectively. |
|
Raw min and Raw max properties are set. |
The converter considers Raw min and Raw max properties and ignores any Low limit and High limit values of the analog variable input. |
|
Only Raw min or Raw max property is set. |
The converter assumes that there is an analog variable set in the input via a dynamic link and ignores the Raw min and Raw max properties. Raw min and Raw max are set to Low limit and High limit of the input analog variable respectively. |
Source
A variable that contains a raw value to be converted.
Output
A scaled value based on the configured linear conversion.
Example

Read from the source node to the parent.
Write from the parent to the source node.
Read from the source node to the parent and write from the parent to the source node.