Create a converter type
Create a converter type and then use a converter instance to transform values in advanced dynamic links.
- In Project view, right-click Converters and select .
-
(optional) Next to the converter object, select
to rename the converter.
- In Properties set the converter property values.
Use the converter type instance to transform values in advanced dynamic links. See Create a complex dynamic link.