Conditional converter
Verify if the source variable value is
True or False.
Properties
| Property | Description |
|---|---|
|
True value |
The value of the expression that is |
|
False value |
The value of the expression that is |
|
Mode |
The direction of the dynamic link:
|
Source
The condition variable (Boolean).
Output
A True or False value.
Example
In the following example, the conditional converter:
-
Sets the text color of a label to green if a switch is selected.
-
Sets the text color of a label to red if a switch is cleared.

Read from the source node to the parent.
Write from the parent to the source node.
Read from the source node to the parent and write from the parent to the source node.