Develop a localized event logger
Create an even logger that displays the interface in the language of a currently logged-in user.
Prerequisites
To develop the project
- Add users.
- Create a login form.
- Create a variable.
- Create a key value converter.
- Create an alarm.
- Create an alarm grid.
- Create a linear gauge.
- Create a database.
- Create an event logger.
- Create a data grid.
- Create a refresh button.
- Edit the localization dictionary.
- Arrange the interface elements.
- Save the project.
Select Run to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.