Create an alarm
Create an exclusive level alarm that warns about exceeded temperature.
- In Project view, right-click Alarms and select .
- In Properties, set High limit to 60.
- Set Auto confirm to True
- Set Message to Maximum temperature exceeded
-
Create a dynamic link between Input variable and .
For more information about dynamic links, see Create dynamic links.