Create a database
Create a database for the event logger.
- In Project view, right-click Loggers and select .
-
Add a database table with the following columns:
Column name Type Value ActiveState_Id Boolean False AckedState_Id Boolean False ConfirmedState_Id Boolean False Time UtcTime Not set Message_it-IT String Message_en-US String Severity UInt16 0 For more information, see Configure a database table.