Create a variable
Create a variable that indicates the current temperature.
-
Create the variable:
- In Project view, right-click Model and select .
-
Hover-over the variable, select
, and enter Temperature.
-
Configure the variable:
- In Properties, select Int32 and select Float.
- Right-click Temperature and select .
- Under EURange, set High limit to 100.