Develop a data logger with an ODBC database
Configure a logger that saves data to an ODBC database.
Note:
Download a sample project: DataLoggerODBC.zip
To run as expected, this sample project requires you to configure the ODBC settings.
Prerequisites
-
Obtain the required details of the ODBC database.
To develop the project
- In Project view, right-click Model and select .
- Create a periodic data logger with an ODBC database that monitors the variable.
- Create the interface elements.
- Arrange the interface elements.
- Save the project.
Select Run to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.