Display an object to a user group
Make a graphical object accessible only for specific users.
Prerequisites
Add a graphical object that you would like to show only to a specific group of users.
For example, create an AdminPane object that is only visible to the Admin group members.
To display an object to a user group
-
In the Project view pane, select the graphical object.
For example, select AdminPane.
-
In the Properties pane, create a dynamic link between the Visible property and .
- TargetGroup
- The group of users that you want to make the graphical element visible for. For example, Admins.
For more information about dynamic links, see Create dynamic links.
The Visibility property of a graphical object has a Boolean value. If the current user at runtime is a part of the selected group, the value of the property at runtime is set to True and the object is visible in the UI.