Configure an alarm event logger
Store logs about past events related to alarms in a database.
- In Project view, right-click DataStores and select .
-
Hover-over EmbeddedDatabase1, select
, and enter AlarmDB.
-
From the toolbar, select
Template Libraries.
- In Libraries, search for Alarms Event Logger.
- Under Components, drag Alarms Event Logger onto Loggers in Project view.
- Select Close.
- In Project view, select AlarmsEventLogger1.
-
In Properties, create a dynamic link between Database and .
For more information about dynamic links, see Create dynamic links.