Configure a widget to display logged alarms
Add a widget that displays historical data about alarms at runtime.
-
From the toolbar, select
Template Libraries.
- In Libraries, search for Alarm History Grid with filter.
- Under Components, drag Alarm History Grid with filter onto Page3 (type) in Project view.
- Select Close.
- In Project view, select FilteredAlarmHistoryGrid1.
-
In Properties, set Horizontal alignment to Stretch.
The object adjusts its width to the container at runtime.
-
Create a dynamic link between AlarmsEventLogger and .
For more information about dynamic links, see Create dynamic links.