FactoryTalk Optix overview
FactoryTalk Optix consists of different software components that run on different parts of your automation system.
Software components
| System | Software | Description |
|---|---|---|
|
Development system |
Integrated development environment with a framework of functional modules for designing and compiling HMI or Internet of Things (IoT) applications. |
|
|
(optional) External code editor |
A third-party code editor for customizing, extending, or adding new features by developing custom C# code.
Tip: Rockwell Automation recommends using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor.
|
|
|
Client system |
An HMI or IoT application developed and compiled in FactoryTalk Optix Studio. |
|
|
FactoryTalk Optix Application Update Service |
Software that is installed on the target device for updating and deploying FactoryTalk Optix Applications from FactoryTalk Optix Studio to the target devices. |
|
| FactoryTalk Optix Runtime Service | Service for running FactoryTalk Optix as a service on the runtime device with or without a user interface. Select this option when installing the Runtime Tools on the target device. |