Configure a digital alarm
Configure a simple Boolean alarm that warns you about issues with Motor1 at runtime.
Tip: By default, a digital alarm triggers when its Input variable equals to 1.
- In Project view, right-click Alarms and select .
-
In Properties, create a dynamic link between the Input variable and Motor1Alarm variable.
For more information about dynamic links, see Create dynamic links.
-
In Message, enter a warning message.
For example, enter Motor1 alarm.