Create a project
Create a Quick start project to develop your FactoryTalk Optix Application.
- Open FactoryTalk Optix Studio.
- Under Create a new project, select Default.
-
In Name, enter the name of the project.
For example, enter QuickStart
- (optional) In Location, edit the directory in which you want to save the project.
- Verify that Use version control is selected.
- Select Create.