Configure a switch to simulate alarms
Configure a switch that simulates Motor1 alarms.
- In Project view, double-click Page2 (type).
- Right-click Page2 (type) and select .
-
In Properties, create a dynamic link between Checked and the Motor1Alarm variable.
For more information about dynamic links, see Create dynamic links.
- In the editor, arrange Switch1 according to your preferences.
At runtime, toggle the switch to trigger an alarm.