FactoryTalk Optix Studio interface
Following is an example of FactoryTalk Optix Studio at design time.
| Item | Name | Description |
|---|---|---|
![]() |
Main toolbar |
Commands that apply to all portions of the user interface. |
![]() |
Project view |
Project information model that displays the content and structure of the project in nodes. A node can be a parent that has child nodes. |
![]() |
Type view |
Object types and variable types on which instances of objects are based. Predefined types are grouped in folders according to their purpose. Custom types are grouped in folders that reflect the structure in Project view. |
![]() |
Output pane |
Messages related to the operation of the FactoryTalk Optix Application. Applications that are running and are connected to FactoryTalk Optix Studio appear on Emulator Output. |
![]() |
Tabs |
Tabs of open objects being modified in the editor. If you hover over a tab to select |
![]() |
Editor toolbar |
Commands that apply to the object type being modified in the editor. |
![]() |
Editor |
Graphic editor for objects. Each editor opens in a new tab and is used for graphic objects and object types, such as tag importers and recipes. |
![]() |
Properties pane |
Properties to set for the selected node in Project view or in the object editor. |
![]() |
Events pane |
Methods with events generated by the currently selected node. See Events. |