Main toolbar
The main toolbar at the top of FactoryTalk Optix Studio contains buttons used by all views in the software.
| Item | Description | Function |
|---|---|---|
| Project |
Opens the Start page. The Start page allows you to create, open, or close a project. |
|
| Save |
Saves the project. Select an option from the list to:
|
|
| Save and Commit |
Saves changes and commit the changes to back them up in the local repository. |
|
| Push to remote |
Pushes saved and committed changes to the remote repository for users to see the latest changes to the project. |
|
| Pull from remote |
Pulls the latest changes from the remote repository to see the latest changes that other users have made. |
|
| View History |
Views the history of changes to the project. Restore any commit to revert to a previous version of the project. |
|
| Undo |
Cancels the last operation. |
|
| Redo |
Repeats the last operation. |
|
| Browse project files |
Opens the project resource window for displaying, importing, or deleting project files such as images, videos, documents, and certificates. |
|
| Template Libraries |
Opens the default and custom libraries and template variables. |
|
| Open .NET Solution |
Opens the .NET project to incorporate additional functionality using custom C# code. |
|
| Open dashboard page |
Opens a configuration dashboard to begin designing your user interface. Select the list to configure the connected device, data logging, and recipes, or manage users and groups. |
|
| Stop |
Stops the application that is running on the client device. |
|
| Run on Emulator |
Compiles, transfers, and runs the application on the selected client device or emulator. Select a different client device from the list. |
|
| VPN |
Opens a VPN connection. |
|
| Remote Desktop |
Opens a Remote Desktop connection. |