Type view
Types are models of objects or variables from which other objects and variables are created. Use Type view to add an object type to the editor to create an instance of that type. Drag the type from a folder in Type view to the window or canvas.
Types are organized into folders by category of object. Example folders include types for the user interface, databases, loggers, alarms, and recipes.