ResourceURI.FromProjectRelativePath(path)
Returns a C# object of the ResourceURI type, with the URIType of ProjectRelative and that contains a relative path to a file than the ProjectFiles folder.
static ResourceUri FromProjectRelativePath(string path);
Arguments
path(string)- A relative path of a file in relation to the ProjectFiles folder.
Returns
ResourceURI- A C# object that contains the path indicated in the argument.
Example
The following example shows an API that returns a C#
projectRelativeResourceURI object of the ResourceURI type that contains the relative path Text1.txt. The object is used as an argument of the .NET WriteAllText API to create a Text1.txt text file inside the ProjectFiles folder.
var projectRelativeResourceUri = ResourceUri.FromProjectRelativePath("Text1.txt");
Log.Info(projectRelativeResourceUri.ProjectRelativePath);
File.WriteAllText(projectRelativeResourceUri.Uri, "Hello world!");