ResourceURI.FromAbsoluteFilePath(path)
Returns a C# object of the ResourceURI type, with the URIType of AbsoluteFilePath that contains an absolute path to a file.
static ResourceUri FromAbsoluteFilePath(string path);
Arguments
path(string)- An absolute path to a file.
Returns
ResourceURI- A C# object that contains the path indicated in the argument.
Example
The following example shows an API that returns a C# applicationRelativeResourceURI object of theResourceURI type that contains the relative path C:\Users\Username\Desktop\Text1.txt.
var applicationRelativeResourceUri = ResourceUri.FromAbsolutePath("C:\Users\Username\Desktop\Text1.txt");