ResourceURI.FromApplicationRelativePath(path)
Returns a C # object of the ResourceURI type, with the URIType of ApplicationRelative that contains a relative path to a file in relation to the ApplicationFiles folder.
static ResourceUri FromApplicationRelativePath(string path);
Arguments
path(string)- A relative path to a file in relation to the ApplicationFiles folder.
Returns
ResourceURI- A C# object that contains the path indicated in the argument.
Example
The following example shows an API that returns a C#
applicationRelativeResourceURI object of the ResourceURI type that contains the Text1.txt relative path. The object is used as an argument of the .NET WriteAllText API to create a Text1.txt text file inside theApplicationFilesfolder.
var applicationRelativeResourceUri = ResourceUri.FromApplicationRelativePath("Text1.txt");
Log.Info(applicationRelativeResourceUri.ApplicationRelativePath);
File.WriteAllText(applicationRelativeResourceUri.Uri, "Hello world!");