Create objects
Use C# APIs to create objects in the FactoryTalk Optix Studio project and return the corresponding C# objects.
The APIs are supplied by the InformationModel class, displayed by the FTOptix.HMIProject module.
Use C# APIs to create objects in the FactoryTalk Optix Studio project and return the corresponding C# objects.
The APIs are supplied by the InformationModel class, displayed by the FTOptix.HMIProject module.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.