Manage translations
Use C# APIs to read or write the translated strings inside the LocalizationDictionary objects.
The APIs are supplied by the InformationModel static class.
LocalizedText class
Every API has an instance of the
LocalizedText C# class among its own arguments, which identifies a key/line or specific string translated in a LocalizationDictionary. It contains the following properties:
NamespaceIndex(int)-
Identifier of the namespace of the project to which the
LocalizationDictionarybelongs.Tip: If theLocalizationDictionaryis in the same NetLogic project, you do not need to specify theNamespaceIndexin the construction of aLocalizedText. TextId(string)- A key with which the translations of a string can be associated.
LocaleId(string)- A locale ID. For example:
en-US. Text(string)- A translated string.