Manage file and resource paths
The ResourceURI static C# class represents the path (URI) of a file or resource inside or outside the project.
ResourceURI class represents the same type of data for the variables. For example, the Path property of an Image object.ResourceURI object properties
| Properties | Data type | Description |
|---|---|---|
|
|
URIType |
The path type of the path contained:
|
|
|
string |
The relative path of a file in relation to the ProjectFiles folder. |
|
|
string |
The relative path of a file in relation to the ApplicationFiles folder. |
|
|
string |
The absolute path of a file external to the project. |
|
|
string |
The absolute path of a generic resource. |
| URIType | ProjectRelativePath | ApplicationRelativePath | AbsoluteFilePath | URI |
|---|---|---|---|---|
|
|
- |
- |
- |
URI (for example, a URL HTTP) |
|
|
Relative path to the ProjectFiles folder |
- |
- |
Absolute path |
|
|
- |
Relative path in relation to the ApplicationFiles folder |
- |
Absolute path |
|
|
- |
- |
Absolute path |
Absolute path |