Manage dynamic links
Use C# APIs to set or remove dynamic links on the variables.
The APIs are supplied by the IUAVariable C# class.
Tip: By default, dynamic links defined in a NetLogic are read-only, whereas dynamic links created with the FactoryTalk Optix Studio UI are read and write.