C# project nodes
The code of a NetLogic represents the project nodes by special C# classes that contain and expose properties.
IUANode class
BrowseName- The name of the node in the project. Cannot be localized.
DisplayName- The name of the node visible in the user interface. Can be localized.
NodeId- The automatically assigned unique ID for the node.
IUAObject class
Displays the properties of any instance of a project object (for example: a graphical object, alarm, driver).
It is an IUANode subclass, which displays all of its properties. It also exposes the ObjectType property, which is a reference to the object type (IUAObjectType class) from which the instance derives.
IUAObjectType class
Displays the properties of any type of a project object (for example: a graphical object, alarm, driver).
It is an IUANode subclass, which displays all of its properties. It also exposes the SuperType property, which is the C# object that represents the object type from which the same IUAObjectType derives.
IUAVariable class
Displays the properties of any project variable instance (base variable, analog variable, controller tag, node pointer).
IUANode subclass, which displays all of its properties. It also exposes the following properties:
ArrayDimensions- The quantity of cells in the array.
DataType- The data type that the variable can contain (for example:
OpcUa.DataTypes.Boolean,OpcUa.DataTypes.Int16). Value- The value of the variable (
UAValueproperty). VariableType- The C# object that represents the type of the variable from which the instance derives.
IUAVariableType class
Displays the properties of any type of a project variable.
IUANode subclass, which displays all of its properties. It also exposes the following properties:
ArrayDimensions- The quantity of cells in the array.
DataType- The data type that the variable can contain (for example:
OpcUa.DataTypes.Boolean,OpcUa.DataTypes.Int16). SuperType- The C# object that represents the variable type from which the same
IUVariableTypederives.
UAValue class
Displays a value. The value can then be converted to and from different types of C# data.
Classes for custom and default objects and variables
A corresponding C# class is available for any custom or default objects and variables. The class is always a subclass of IUAObject or IUAVariable, to which any properties specified in the type are added.
For example, if a Motor object type is created in FactoryTalk Optix Studio with the Speed and Acceleration properties, the Motor C# class is automatically created with the Speed, SpeedVariable, Acceleration, and AccelerationVariable properties.
C# default class types are defined in FTOptix modules. When you save the project, FactoryTalk Optix Studio creates C# classes that correspond to custom types.
Object properties
- A property which name equals to the
BrowseNameof the property -
Represents the value of the property (for example:
"Current speed is: "). The value of the property is that of the same C# property (for example, string data type forText).For example, the
Textclass for theTextproperty of aLabelobject. - A property of the
IUAVariabletype which name consists of theBrowseNameof the property and theVariable
suffix -
Represents the OPC UA node of the property. It is useful for setting dynamic links and other instructions that require access to the
IUAVariableclass of the property.For example, the
TextVariableproperty corresponds to theTextproperty of aLabelobject.