C# API reference
Use C# APIs to create logics that manipulate project nodes, variables, log messages, dynamic links, aliases, paths, and translations.
The complete lists of tasks that can be used from the C# API reference include:
- Return known nodes
- Return nodes by searching
- Add or remove nodes
- Create objects
- Create variables
- Read or write field variables
- Keep field variables synchronized
- Write log messages
- Manage dynamic links
- Manage aliases
- Manage file and resource paths
- Session activity log and audit
- Manage translations
- Serial Port API